Traceparts

ANT Antriebstechnik develops online configurator with TraceParts

ANT will be presenting its web configurator for screw jacks and high-speed screw jacks right in time for the Motek automation trade fair

The screw jacks and high-speed screw jacks from ANT Antriebstechnik operate as the kinematic core of many innovative automation process modules. The company, based in Schweinfurt, Germany, has recently significantly expanded its selection of types and models featuring in this range in its portfolio. It is currently collaborating with CAD-content platform specialist TraceParts in developing a browser-based online configurator for designers, which will be released for this year’s Motek trade fair. ANT will present it in Stuttgart in Exhibition Hall 1, Booth 1214.When it comes to the highly efficient conversion of rotary movements into linear movements, the screw jacks and high-speed screw jacks developed by ANT Antriebstechnik are among the top solutions available in the automation components market. Over the past two years, the company has expanded its offering in this product segment with numerous models. In addition, to ensure that designers and developers have quick and easy access to this new selection, ANT is currently having a product configurator developed by TraceParts, which will be presented at this year’s Motek trade fair. 

The online provision of all available standard versions and, in particular, the option of transferring the relevant CAD data from the new configurator directly into established CAD systems such as Solidworks, ProE, Catia, Inventor, and many others, will significantly improve the availability of our screw jacks and high-speed screw jacks for users and customers.

Mathias Keul, ANT Antriebstechnik Managing Director

Shortcut to a special solution

However, the new web configurator will do more than just simplify the selection and design work involved with the many standard versions of ANT’s screw jacks and high-speed screw jacks. In fact, the online tool is designed in such a way that, once a configuration is completed, it offers the option of both submitting a specific request for a quotation and preparing the continuing process involving the individual optimization of the selection made by ANT engineers.

Based on the customers’ online configurations, we can – using our flexible production structures – implement special application-specific requests very quickly and easily.

Mathias Keul, ANT Antriebstechnik Managing Director

At its Motek Booth 1214 in Hall 1 of the Stuttgart Exhibition Center, ANT will give designers, developers and buyers of plant manufacturers, and system integrators an insight for the first time into how its new online configurator works. At its booth, the company will also be presenting, for instance, a number of versions of the screw jacks in the NM range (trapezoidal spindle) along with the high-speed screw jacks in the NG range (ball or trapezoidal threads) and the high-performance NH type screw jacks (ball screws). 

About ANT Antriebstechnik

ANT Antriebstechnik operates according to a two-track strategy. The company supplies plant manufacturers that want to run their automation projects in-house with linear modules, screw jacks, and ball screws based on components selected from the catalog or using special customer-specific products. ANT provides all other customers with its one-stop-shop range of services, from planning and design to assembly and acceptance of total system solutions. As part of all this, in addition to the Bosch Rexroth portfolio, the company also uses its own development and production capacities, as well as the flexible opportunities for collaboration offered by its partner concept. This allows ANT not only to produce customer-specific modified linear guides and gearboxes, but also entire process modules for gantry systems and assembly devices right up to complete processing, assembly, handling, and testing systems.

About the Author

Stefan Kolb
Stefan Kolb

Online Marketing Manager, TraceParts