Traceparts

Free Trial Licenses Of TraceParts 3D Library For CATIA V5 To Be Offered During COE 2005 Annual PLM Conference & TechniFair in Phoenix, USA.

First US-based exhibition since TraceParts acquisition of web2CAD/PowerPARTS European business will demonstrate more than 100 million 3D native CATIA models.

COE logoSaint Romain (France) – March 14, 2005 – TraceParts will be offering 30-day evaluation licenses of its parts library seamlessly integrated to CATIA V5 at the COE 2005 Annual PLM Conference & TechniFair (booth #316), taking place March 20-23, in Phoenix, Arizona.
TraceParts was the first Parts Library to join the DASSAULT SYSTEMES‘ Software Community Program (SCP) as a Partner in October 2001. Through this development partnership TraceParts is still the only CAA V5 Partner to complement native parts catalogs by delivering to CATIA V5 users more than 25 million parts directly accessible from DS 3D PLM solutions. TraceParts‘ commitment to CATIA customers and business partners is also being reinforced through this 3rd participation to the COE Technifair.

 

TraceParts for CATIA Interface - Aerospace standards

 

TraceParts leverages the V5 architecture to develop an extensive library of international standard CATIA-native 3D parts. Customers from all industries, and especially Industrial Machinery, Tooling, Automotive and Aerospace will benefit from all the most commonly used components in mechanical design from the largest names of the mechanical industry: Asco Joucomatic Numatics, BOSCH, BOUTET, CHAMBRELAN, CSR, ENOMAX, GENUSTECH, HERVIEU, HP SYSTEMS, INA, KV, LEGRIS, NSK, PARKER, PARVEX, PAULSTRA, QUIRI, RABOURDIN, RÖMHELD, SIAM-RINGSPANN, SKF, SNR, SPEEDY BLOCK, SUMER, TELEMECANIQUE, …

 

TraceParts completely eliminates the time consuming process of finding and modeling international standard and manufacturers‘ components. The time saved in this way allows the designer to spend more time on the more critical stages of the design process.

 

Free TraceParts evaluation CD for all the COE 2005 attendees

Each COE exhibition attendee will receive a free 30-day trial CD and a product brochure in their COE bag.

 

Supply your engineers & designers with high quality models at their fingertips and let them concentrate on adding value to your company’s products!

– Content :

More than 25 million components straight from the leading parts manufacturers in the world and international standards. The content includes such components as: fasteners, shaft ends, keys, pins, gears, bearings, cylinders, flanges, reducers, elbows, electric motors and structural sections, and also included are detailed technical documents regarding the individual products. The content of TraceParts is relevant to all mechanical designers in the tooling, machinery, automotive and aerospace industries.
Aerospace MS/NAS/NASM standard parts are available now including plate nuts, bolts, screws, studs, washers & rivets

 

– Integration :

TraceParts is run directly from within CATIA V5 and the selected components are automatically inserted into the current session, with all their Bill Of Material attributes attached as .CATPart properties (part name, reference, manufacturer, standard, mass, …). When applicable, V5 native features such as threading parameters, publications and materials are also automatically provided.

 

– Power :

Several search engines are included in TraceParts as well as 2D and 3D viewers, these features mean that time is saved when selecting components as the right component is found from the first time.

 

– Customization :

TraceParts database can be linked to an external source of data in order to associate customized ERP/PDM information (internal references, prices, status, naming, …) to the standard attributes directly coming from manufacturers‘ catalogs.

 

– Updates :

Downloads of product updates and new parts catalogs are available through an exclusive maintenance contract. Maintenance customers can directly influence the product development and the modeling of new catalogs.

– Intranet/Extranet versions of TraceParts can be customized to match specific content requirements such as US aerospace and automotive parts.

 

About TraceParts

TraceParts S.A. is a leading software company which belongs to the Trace Software Group, founded in 1989 to develop and market original solutions to help CAD users to increase their productivity through both Online and CD-based Parts Libraries, e-catalogs and product configurations.
TraceParts develops a very innovative technology which relies on strong and long term partnerships with all the main CAD vendors in the world: DASSAULT SYSTEMES (CATIA, SOLIDWORKS and Spatial), AUTODESK (AutoCAD, Inventor, Mechanical Desktop), PTC (Pro/ENGINEER), THINK3 (thindkesign), MISSLER SOFTWARE (TopSolid), UGS (Unigraphics, Solid Edge). TraceParts was the first and is still the only Parts Library in the world to get the CAA V5 Software Partner label from DASSAULT SYSTEMES, therefore delivering a seamless integration with CATIA V5.
TraceParts catalogs come from partnerships with major parts manufacturers and distributors including Asco Joucomatic Numatics, BOUTET, CHAMBRELAN, CSR, ENOMAX, GENUSTECH, HERVIEU, HP SYSTEMS, INA, LEGRIS, NSK, PARVEX, PAULSTRA, QUIRI, RABOURDIN, SIAM-RINGSPANN, SNR, SUMER, TELEMECANIQUE …
TraceParts is the number one Parts Library in France, Italy, Spain, UK, Benelux and Turkey, with more than 20,000 commercial seats sold in 35 countries to companies such as MICHELIN, NORTHROP GRUMMAN, SCHNEIDER, AIRBUS, DYSON, COMAU, DELPHI KOREA, ALCATEL, ABB, ALSTOM, NESTLE, BOBST, TECHNIP, OLIVETTI, …
web2CAD TraceParts GmbH is a subsidiary of TraceParts S.A., founded in 2004 in Germany to support the many PowerParts customers and to massively extend the business of Parts Libraries.
The combination of both TraceParts and PowerParts European content forms one of the most extensive and most widely used CAD Parts Library in the world, with more than 190 parts catalogs and 100 million CAD drawings which can be accessed by the 200,000 registered users of the Internet portals PowerParts on Web and tracepartsonline.net.
More details about TraceParts and web2CAD can be found on the Web: www.traceparts.com

 

TraceParts is being distributed in North America by LionHeart Solutions, Inc.

 

About LionHeart Solutions, Inc.

LionHeart Solutions was formed in 1999 to offer Consulting & Design Services to companies using Dassault Systemes‘ CATIA Software. Their services include consulting on implementation plans, design methodology, validation of system architecture & hardware configurations, benchmarking, installation & administration to providing a complete turnkey installation. Check out their services page for further details:www.lionheartsolutions.com

 

TraceParts is a trademark of TraceParts S.A. All other products and company names are trademarks or registered trademarks of their respective owners.

Über den Autor

TraceParts
TraceParts

TraceParts ist einer der weltweit führenden CAD-Content-Plattformen in den Bereichen Ingenieurwesen, Industrieanlagen und Maschinenbau. TraceParts bietet Hunderten von Kunden aus den unterschiedlichsten Branchen und Größen hochgradig gezielte Marketingservices zur Leadgenerierung über eine leistungsstarke Cloud-basierte API und SaaS-Anwendungen wie 3D-Bauteilbibliotheken, Produktkataloge und Konfiguratoren.